SLAU893B October 2023 – July 2024 MSPM0C1103 , MSPM0C1103-Q1 , MSPM0C1104 , MSPM0C1104-Q1
When using the Motorola frame format, the CDMODE bit can be set to use the CS3/CD line as signal to distinguish between Command and Data information. This is often used for LCD or data storage devices.
The CTL1.CDMODE can be written with a value of 1-14 to specify the number of bytes and the CD line will go low for the given numbers of bytes which are sent by the SPI, starting with the next value to be transmitted. After the number of bytes are transmitted the CD will go high automatically. If a value of 0xF is set the C/D stays low permanently, a value of 0 set the CD line to high immediately after the current character has been transmitted.
This option is only available in controller mode. CTL1.CDENABLE can only be updated when the SPI module is disabled, CTL1.CDMODE can be updated between the different data packages. The counter will be reset with CDENABLE or SPI ENABLE set to disabled. Before setting a new value in CTL1.CDMODE the status of the FIFO should be checked to be empty and the SPI should be in Idle mode.
When writing a new value into CTL1.CDMODE, the internal counter will be reset and the new value will be used for counting. If the counter did count down to 0 and another command package should be sent the CDMODE needs to be set first again, otherwise the next data is send as data with the CD pin signaling data mode.