Some timer modules have a shadow load and shadow compare register feature which gives the user the flexibility of holding the update of load and CC values until a certain event occurs. This is useful
in timing-critical applications where PWM control signals need to be updated with correct timings, such as duty cycle updates. Refer to the timer features for specific configurations of the TIMx modules.
Note: See
Section 15.1.3 and the device-specific data sheet for TIMx instances that support Shadow Load and Shadow Compare.