SLAU893B October 2023 – July 2024 MSPM0C1103 , MSPM0C1103-Q1 , MSPM0C1104 , MSPM0C1104-Q1
In AUTO mode, the sample signal is generated synchronous to the sampling clock (SAMPCLK) and can be programmed using an internal sampling timer to determine the duration of the sampling window. The sample timer is 10-bits wide and there are two sample time compare registers (SCOMPx) available to account for various source impedances to measure signals from. One of these two SCOMP registers can be selected using the STIME bit in the MEMCTL register.
There is a 2-3 cycle latency from when the sampling is triggered and when the sampling period starts. This latency can be bypassed by setting ULPCLK as the source for ADCCLK. This synchronization bypass feature is very useful for deterministic sampling
Figure 9-2 shows the ADC sample and conversion timing diagram when the ADC is configured in AUTO sampling mode.