SLAU893B October 2023 – July 2024 MSPM0C1103 , MSPM0C1103-Q1 , MSPM0C1104 , MSPM0C1104-Q1
The code region contains the flash memory used to store executable code and data. Accesses to the flash memory from the CPU through the code region are processed through the AHB bus matrix to the flash read interface directly. See Section 5.2.3.1 for the detailed flash memory map.
The code region also contains the read-only memory (ROM) used for the TI device boot code and the bootstrap loader. Note that not all MSPM0Cxx devices have the bootstrap loader. See the device-specific data sheet to determine if the bootstrap loader is present. The ROM is only available during the initial device boot process.