SLIA096 January 2022 DRV5021 , DRV5021-Q1 , DRV5023 , DRV5023-Q1 , DRV5032 , DRV5033 , DRV5033-Q1 , TMAG5123 , TMAG5123-Q1 , TMAG5124 , TMAG5124-Q1 , TMAG5131-Q1 , TMAG5231 , TMAG5328
All trademarks are the property of their respective owners.
Working with complex machines such as vehicles, involves various tactile controls. Often these controls provide three states of operation, such as initiating a car door to lock, unlock, or remain idle and also when raising, lowering, or maintaining:
In addition to these, there are likely many more possible applications and these need not be strictly relevant to an automobile. One particular type of tactile control that can be utilized for such state selection is the Rocker Switch. This document dives into the basic operating principles and shows the design process for one possible version of a rocker switch. Challenges in the design process are also documented.
Figure 1-1 summarizes the design flow presented in this document.
A rocker switch can be generalized into four basic mechanical components: a base, axle, springs, and a rocker. In this case the base holds the axle and has cantilevers that serve as springs for returning the rocker back to the resting state when the user is not applying force. While these cantilevers are not the primary focus in this design, note that traditional metal spring alternatives were intentionally avoided as many are typically composed of iron which can influence the magnetic field shape from a nearby magnet and thereby complicate design.