Install the EVM using the following
steps:
- Attach a USB2 or USB3 cable from
a Host PC Type-A connector to the Type-B connector (P1) of the
TUSB211RPTREVM.
- Attach a USB device either via
cable or directly plugged into the Type-A receptacle connector (P2) on the
TUSB211RPTREVM:
- When LED D2 is lit, this
indicates a USB device connection.
- When LED D1 is lit, this
indicates a USB High-Speed connection with the TUSB211A active.