SLOA246B January 2018 – March 2019 TRF7964A , TRF7970A
TI has obsoleted the TRF7970AEVM. This was done as the firmware provided with in the TRF7970AEVM was out-of-date and the MCU that was used on the board did not have the required flash space to support TI's new full NFC stack.
For all applications concerning evaluation of the TRF7970A, consider the options in Section 1.3.
For applications concerning the RF430FRL152HEVM and the GUI associated with it, the following hardware and software act as the replacement for the TRF7970AEVM:
The binary image can be flashed onto the MSP-EXP430G2 LaunchPad development kit using CCS UniFlash.