SLOA246B January 2018 – March 2019 TRF7964A , TRF7970A
The concept of NDEF is to create a universal format for how to store data across all NFC tags. This allows NFC devices such as smartphones to have a standard for how to read data across each NFC technology type despite varying memory structures and features.
The advantage of using NDEF is that any NFC-compliant device is able to read and write to an NDEF formatted tag allowing for excellent interoperability with a large number of devices and tags in the market.
NDEF should be leveraged for applications in which any of the following is desired:
NDEF may not be an ideal choice for some applications such as: