SLOA343 August 2024 TPS543820 , TPS543A22 , TPSM843620 , TPSM843A22
The following data was taken in the CISPR Chamber with CISPR32 pre-compliant setup. These results are not officially CISPR certified. The table below shows a summary of the experimental setup for each set of tests. A photo of the setup is shown in Figure 4-1. The results show a significant improvement in the radiated emissions, showing that EMI can be heavily reduced by changing only the layout.
IC | Vin | Vout | Iout | Switching Frequency |
---|---|---|---|---|
TPS543820 | 12V | 1.2V | 8A | 500kHz |
TPSM843620 | 12V | 1.2V | 6A | 500kHz |
TPS543A22 | 12V | 1.2V | 10A | 500kHz |
TPSM843A22 | 12V | 1.2V | 10A | 500kHz |