SLUA778A June 2016 – July 2016 UCC21520 , UCC21520-Q1 , UCC21540
The propagation delay mismatch will introduce internal shoot-through if the two output channels are paralleled. Figure 2 shows the simplified circuit diagram with UCC21520 two output channels in parallel driving a heavy load. In this example, it is assumed that the channel A turn-on happens earlier than channel B, or channel A turn-off later than channel B. The red dotted line shows the shoot-through path which shorts VDD to ground with very small impedance, which is typically 1.5 Ω combining pull-up and pull-down resistance. Therefore, there will be large current flow through the gate driver device, and will result in additional internal heat. The estimated loss per cycle can be calculated by:
where
To make sure UCC21520 two channels can be used in parallel, it is essential to quantify the delay matching data at different VDD voltage and temperature.