SLUAA32A October 2020 – September 2021 BQ769142 , BQ76922 , BQ76942 , BQ76952
The BQ769x2 has commands that support raw ADC readings to support calibration of voltage, current, and temperature readings. The following sections will outline steps required for the calibration of different measurement types, the commands and subcommands needed for each of the readings, and the RAM parameters where calibration data can be stored.