One of these properties of GaN can
prove to be extremely valuable in one of the most efficient power converter
topologies that addresses thermal and energy storage challenges: the Active-Clamp
Flyback (ACF).
Compared to the traditional flyback,
ACF greatly saves on power loss by:
- Eliminating losses in the
traditional snubber clamp with zero-clamp-loss
- Reducing switching losses
with Zero-Voltage-Switching (ZVS)
Both of these mechanisms are carried out by the configuration of the switching
devices, magnetizing inductance, clamp capacitors, and parasitic elements, such as
leakage inductance and device capacitance. The fundamental operation of these power
loss-saving mechanisms is explained in more detail in
Section 3.1 and
Section 3.2.