SLUAAP5 july   2023 UCD3138 , UCD3138064 , UCD3138064A , UCD3138128 , UCD3138128A , UCD3138A , UCD3138A64

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Why Lockup Can Occur
  5. 2Reasons for Lockup
    1. 2.1 Wrong Code in the load.asm
    2. 2.2 Misoperation with TI GUI
    3. 2.3 zero_out_integrity_word Function Fails
    4. 2.4 PMBus Communication Fails
    5. 2.5 Unexpected Occurrences
  6. 3How to Avoid a Lockup
  7. 4Unlock with JTAG
    1. 4.1 Enable JTAG Functionality
    2. 4.2 New Target Configuration in CCS
    3. 4.3 Clear the Flash
  8. 5Summary
  9. 6References

Summary

A lockup can occur when there is a valid checksum that cannot be cleared, which can be caused by either an incorrect download process or firmware with bugs. To avoid a lockup, check the possible reasons listed and follow the instructions before programming with checksum. If the device is locked, but the firmware is executing normally and PMBus works, the device is able to recover with JTAG. Otherwise, there is no way to save.