SLUAAP5 july   2023 UCD3138 , UCD3138064 , UCD3138064A , UCD3138128 , UCD3138128A , UCD3138A , UCD3138A64

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Why Lockup Can Occur
  5. 2Reasons for Lockup
    1. 2.1 Wrong Code in the load.asm
    2. 2.2 Misoperation with TI GUI
    3. 2.3 zero_out_integrity_word Function Fails
    4. 2.4 PMBus Communication Fails
    5. 2.5 Unexpected Occurrences
  6. 3How to Avoid a Lockup
  7. 4Unlock with JTAG
    1. 4.1 Enable JTAG Functionality
    2. 4.2 New Target Configuration in CCS
    3. 4.3 Clear the Flash
  8. 5Summary
  9. 6References

Unlock with JTAG

If the device cannot be reprogrammed, but the firmware is executing normally and the memory debugger read or write functionality works, there is a way to unlock with JTAG.