SLUU885C March 2012 – June 2024 UCD3138 , UCD3138064 , UCD3138064A , UCD3138128 , UCD3138A , UCD3138A64
On the lower left corner of that shown in Figure 13-2, there are four tabs, called Configure, Design, Monitor and Status. Clicking each tab brings a unique page to the front of that page. The clicked tab is highlighted in blue. Figure 13-2 shows Monitor tab was clicked. The page shows all variables in monitoring with UCD3138 single-phase PFC. These variables are communicated through PMBus. Adding more variables in Monitoring is possible but has to be executed through the firmware code change and re-compile process.