SLUUBD5D September 2019 – February 2022 UCC12040 , UCC12050 , UCC12051-Q1
Test points for VINP, VISO, and SYNC are provided on the EVM.
To get the cleanest measurement of output ripple using an oscilloscope, use probe tip with a ground spring.
This reduces the added noise that is introduced when using the longer alligator clip style ground lead. Figure 5-1 shows a picture illustrating how these test points are best used.
Comparison scope shots between the two grounding methods are shown in Figure 5-2.