The current bench setup diagram includes the function generator and oscilloscope connections.
Use the following connection procedure and also
use Figure 5-2 as a
reference:
Make sure all the output of the function generator, voltage source are disabled before connection;
Function generator channel-A channel applied on INA
(TP3) ←→ GND (TP14) as seen in Figure 5-2;
Function generator channel-B channel applied on INB
(TP5) ←→ GND (TP6) as seen in Figure 5-2. For the
UCC20520EVM, INB, J-INB and TP15 are not installed because the UCC20520 is a
single PWM input, dual-channel output Iso-Driver;
Power supply #1: positive node applied on VCCI (TP1), and negative node applied on GND (TP2);
Power supply #2: positive node connected to input of DMM #1 and DMM #1 output connected to VDDA (TP17), negative node connected directly to VSSA (TP19);
Power supply #3: positive node connected to input of DMM #2 and DMM #2 output connected to VDDB (TP20), negative node connected directly to VSSB (TP22);
Oscilloscope channel-A probes TP14, smaller measurement loop is preferred;
Oscilloscope channel-B probes TP16, smaller measurement loop is preferred;