SLVAFC5 March   2022 TPS629210 , TPS629210-Q1

 

  1.   Trademarks
  2. 1Inverting Buck – Boost Topology
    1. 1.1 Concept
    2. 1.2 Output Current Calculations
    3. 1.3 VIN and VOUT Range
  3. 2Digital Pin Configurations
    1. 2.1 Enable Pin
    2. 2.2 MODE/S-CONF Pin
    3. 2.3 Power Good Pin
  4. 3Design Considerations
    1. 3.1 Input Capacitor Selection
    2. 3.2 Output Inductor Selection
    3. 3.3 Stability Limits and Output Capacitor Selection
  5. 4Layout Considerations
  6. 5How to Modify a Buck to Inverting Buck-Boost?
  7. 6Typical Performance and Waveforms
  8. 7Conclusion
  9. 8References

How to Modify a Buck to Inverting Buck-Boost?

To achieve the inverting function, the output terminals are swapped such that VOUT becomes GND and the GND terminal becomes -VOUT. Everything was GND is now labeled - VOUT. The modification shown in .Figure 5-1

  • The reference designators are identical between buck and inverting buck boost, except for the input capacitors C1, C2 and C3 whose connections need to be changed
  • Remove input capacitor C1, C2 and C3 from the EVM, but save them to re-install later
  • Install 2 pcs 22 μF, 10V ceramic output capacitors at C6 and C7. Might add more to reduce output ripple and improve loop stability.
  • Change the value of R1 and R2 to set the appropriate output voltage

GUID-20220207-SS0I-FW2R-HLT8-ZFZGDBLHKQVW-low.png Figure 5-1 Buck EVM Before Modification
Installing the input capacitor C1, C2 and C3 guidance shown in Figure 5-2
  • Because existing input GND pads of input capacitors C3 are not the correct electrical location on existing EVM. So put a electrical tape to cover that GND pad of C3 to avoid wrong connection.
  • The existing pad for VIN connection of C3 is used and a wire is added to complete the connection to GND, which is Vout on the PCB
  • Re-install C1, C2 and C3 as highlighted in red square area
  • Input supply can be applied between VIN and GND, which is VOUT on the PCB
  • Load can be applied between -VOUT and GND
GUID-20220207-SS0I-WK9H-VZJT-F6C0QF9VMJT6-low.png Figure 5-2 Inverting Buck-Boost EVM After Modification