SLVUCZ9 July 2024 DRV81004-Q1 , DRV81008-Q1 , DRV81620-Q1
The DRV81xxx-Q1 family of devices is designed to drive low-side, and high-side loads. The following section explains how each EVM must be configured to drive the desired load.
J1: Connects 3.3V to VDD.
The DRV81004-Q1 has four low-side switch outputs. Loads must be connected across blue output terminals OUT0-OUT3 accordingly.
The DRV81008-Q1 has eight low-side switch outputs. Loads must be connected across blue output terminals OUT0-OUT7 accordingly.
The DRV81080-Q1 has eight high-side switch outputs. Loads must be connected across blue output terminals OUT0-OUT7 accordingly.
The DRV81602-Q1 has six configurable outputs that can be used as a high-side switch or a low-side switch. If an output is being used as a high-side switch then the yellow jumpers need to be populated and the load connected from OUTx_S to GND. If driving low-side loads, then the purple jumpers need to be populated and the corresponding load connected from OUTx_S to VM. If an output is being used as a low-side switch then the purple jumpers need to be populated and the load connected from OUTx_D to VM.
The DRV81242-Q1 has two configurable outputs that can be used as a high-side switch or a low-side switch. If an output is being used as a high-side switch then the yellow jumpers need to be populated and the load connected from OUTx_S to GND. If driving low-side loads the purple jumpers need to be populated and the corresponding load connected from OUTx_S to VM. If an output is being used as a low-side switch then the purple jumpers need to be populated and the load connected from OUTx_D to VM.
The DRV81620-Q1 has six configurable outputs that can be used as a high-side switch or a low-side switch. If an output is being used as a high-side switch then the yellow jumpers need to be populated and the load connected from OUTx_S to GND. If driving low-side loads the purple jumpers need to be populated and the corresponding load connected from OUTx_S to VM. If an output is being used as a low-side switch then the purple jumpers need to be populated and the load connected from OUTx_D to VM.
All EVMs require a VDD power supply for digital logic. Some of the configurable and high-side switch drivers require a jumper placement for additional power supply. See the table below for a description the device and jumper requirements.
Device | Jumpers | Description |
---|---|---|
DRV81004 | J1 | Connects 3.3V to VDD |
DRV81008 | J1 | Connects 3.3V to VDD |
DRV81080 | J1 | Connects 3.3V to VDD |
J3 | Connects VM to VM1 | |
J4 | Connects VM to VM2 | |
DRV81602 | J1 | Connects 3.3V to VDD |
DRV81242 | J1 | Connects 3.3V to VDD |
J18 | Connects VM to VM_HS | |
DRV81620 | J1 | Connects 3.3V to VDD |