SLYA085 December 2023 TMAG6180-Q1
The variation shown in Figure 1-3 is particularly helpful if the sensor is setup in the format of a Wheatstone bridge, shown in Figure 2-1. This particular configuration produces two parallel resistor dividers with elements physically orthogonal to each other. The variation in resistance results from the incident magnetic field producing a sinusoidal response as the field travels through a full rotation, balancing the structure with AMR elements with equally sized resistances along each axis.
What is particularly noteworthy about the response of the sensing element is that the output varies with cos2Ɵ. As a result, a typical AMR sensor produces two output cycles per revolution and a single Wheatstone bridge only directly resolves a physical rotation of 90°.
Given the response of the sensor to the rotating magnetic field, creating an electrically orthogonal set of sinusoidal outputs by integrating a second Wheatstone bridge rotated 45° is possible.
Together, the outputs represent sine and cosine, and can then be used to calculate an arctangent with a full 360° response for every 180° of mechanical rotation.
TMAG6180-Q1 and TMAG6181-Q1 take advantage of this sensing technology by combining a fast, two-dimension, Hall-effect latch to create an AMR sensor capable of detecting quadrant and extending the sensing range from 180° to the full 360°. TMAG6180-Q1 generates Q0 and Q1 outputs which can calculate absolute angle. TMAG6181-Q1 provides a turns counter that can increment or decrement at each quadrant change. This counter tracks the relative angle from power-on and absolute angle is possible if the turns counter is always initialized within the same 180° range.
Automatic Gain Control (AGC) in both devices is set to produce outputs with a peak to peak amplitude of 0.6 × Vcc with the output centered at Vcc/2, irrespective of the input magnetic field strength. The sensor adjusts the applied gain to maintain a constant output level following Equation 2 when changes in the magnetic field produce vector magnitude drift.
The calculated signal typically swings between ±0.6 × Vcc when measured differentially. For example, when Vcc = 3.3 V, each output signal can vary between 0.66 V and 2.64 V, and when taken differentially the resulting signal ranges between ±1.98 V.