SLYU058D May   2021  – February 2024 TMAG5173-Q1 , TMAG5273

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Overview
    1. 1.1 Kit Contents
    2. 1.2 Related Documentation From Texas Instruments
  5. 2Hardware
    1. 2.1 Features
  6. 3Operation
    1. 3.1 Quick Start Setup
  7. 4EVM Operation
    1. 4.1 Setup
      1. 4.1.1 Driver Installation
      2. 4.1.2 Firmware
        1. 4.1.2.1 Updating Firmware on SCB
      3. 4.1.3 GUI Setup and Usage
        1. 4.1.3.1 Initial Setup
        2. 4.1.3.2 GUI Operation
    2. 4.2 Rotate and Push Demo
    3. 4.3 Joystick Demo
    4. 4.4 Direct EVM Serial Communication
  8. 5Circuitry
    1. 5.1 TMAG5x73 EVM Components
    2. 5.2 SCB LEDs
  9. 6Schematics, PCB Layout, and Bill of Materials
    1. 6.1 Schematics
    2. 6.2 PCB Layout
    3. 6.3 Bill of Materials
  10. 7Revision History

Quick Start Setup

GUID-20210826-SS0I-4CGX-NR7H-WVNPJ4JCDCPB-low.jpg Figure 3-1 TMAG5x73 EVM With A1 and A2 Parts of Board Still Joined Together

To set up and use the EVM, follow these steps:

  1. Gently flex the panel at the score line shown in Figure 3-1 to split the board in half for a more compact form factor. This split provides separate boards for the TMAG5x73A1 and TMAG5x73A2 portions of the original board.

  2. Download and install the driver as a one-time step per PC: http://www.ti.com/tool/download/sbac253
  3. Attach the EVM to the Sensor Control Board (SCB). To evaluate the TMAG5x73A1 on the EVM, attach header J1 of the Sensor Controller board to header J1_A1 of the EVM (see Figure 4-1). To evaluate the TMAG5x73A2 on the EVM, attach header J1 of the Sensor Controller board to header J1_A2 of the EVM (see Figure 4-2).
  4. Use a USB cable to connect the SCB to a PC
    1. Insert the micro USB cable into the USB receptacle J2 that is on the SCB Controller onboard.
    2. Plug the other end of the USB cable into a PC.
  5. Access the GUI in either the Google Chrome® or Firefox® browser by clicking on the following link: https://dev.ti.com/gallery/info/PositionSensing/TMAG5x73EVM_GUI/
  6. To quickly view results on the GUI, do the following:
    1. Modify the MAG_CH_EN bits in the SENSOR_CONFIG_1 register to enable the desired channels to read from. The GUI has drop-down boxes to configure these bits when the SENSOR_CONFIG_1 register is selected in the register tab of the GUI.
    2. Select the desired result plots under the Results to collect/show box in the Results Data tab, and press Collect Data to trigger the read.
    These two steps are the minimum steps needed to see results in the GUI. However, this assumes that the default register settings are used for the other registers. For more custom settings, modify the corresponding register bits according to the system requirements.
  7. Apply a magnetic field to the sensor by doing one of the following:
    1. Wave the included handheld magnet around the sensor.
    2. Attach either the Rotate & Push module or the Joystick module to the EVM (see Section 4.2 and Section 4.3). For more details on how to use these modules, see Section 4.2 and Section 4.3.
  8. Observe the outputs in the GUI.