SLYU064A June 2023 – December 2023 TMAG3001 , TMAG5170 , TMAG5170-Q1 , TMAG5170D-Q1 , TMAG5173-Q1 , TMAG5253 , TMAG5273
Having established general expectations of what output is needed for the design, the iterative process of finding the exact placement regions can now be executed. TI offers a Magnetic Sense Simulator to facilitate this process. This tool has a main menu, where the user can specify the type of magnet movement. The user selection then takes them to a sub-menu with entries to specify magnet placement, sensor placement, range of motion, and device of interest. Figure 2-9 shows the top menu and the Rotation movement sub-menu.
For the two-sensor thumbstick, the inputs required for the desired behavior are shown in Figure 2-11.