SLYU064A June 2023 – December 2023 TMAG3001 , TMAG5170 , TMAG5170-Q1 , TMAG5170D-Q1 , TMAG5173-Q1 , TMAG5253 , TMAG5273
Offset corresponds to the magnet not being centered properly over the device sensing element, indicated by the blue box in Figure 2-25. Offset along the y-axis as defined in Figure 2-25, is not as bad as offset along the x-axis or z-axis. Increasing the offset along the z-axis decreases the field strength measure by the device. Whereas offset along the x-axis shifts the field characteristic and decreases the usable linear range.