SNIU028D February 2016 – September 2020 UCD3138 , UCD3138064 , UCD3138064A , UCD3138128 , UCD3138A , UCD3138A64
FILTERMUX controls some inputs to the filters. It selects which Front End provides the error signal to each filter. FILTERMUX also selects values for multiplication in the filter output stage (see Section 4.2.6). For this function, FILTERMUX works together with the PERIOD_MULT_SEL and OUTPUT_MUL_SEL fields in the FILTERCTRL register.
For each Filter, FILTERMUX selects one of each from:
Then OUTPUT_MULT_SEL bits select from these preselected values. OUTPUT_MULT_SEL can select any of the 4 inputs. PER_MULT_SEL can only select from Period or KComp.