Purpose: To ensure correct PHY transmitter output voltage levels.
Pass Condition: Voltage Levels are to be within:
Equation 1.
Equation 2.
Equation 3.
Equation 4.
Equation 5.
Where Average of Peak Voltage A and B is defined as .
Specific Test Setup: Verify the correct test fixture connections. Note that some Ethernet compliance software can run Template and Peak Voltage Tests simultaneously.
Note: Some older versions of Ethernet compliance software use an incorrect formula for determining symmetry within 1% between Peak Voltage A and B. This can result in 2x the actual percent value, failing the test case. Hence any failing result needs to be double checked using (3).