SNLA421 December 2022 DS320PR810 , SN75LVPE5412 , SN75LVPE5421
This application note describes the results of compliance and electrical testing with DS320PR810 (PCI Express Gen 5.0 8-channel Linear Redriver) and high-level redriver tuning guidance.. The intended audience for this document includes hardware engineers using DS320PR810 in their design. Please note that the procedures and testing results highlighted in this document also apply to the SN75LVPE5412 (PCI Express Gen 5.0 4-channel Linear Redriver with Integrated 1:2 Demux) and SN75LVPE5421 (PCI Express Gen 5.0 4-channel Linear Redriver with Integrated 2:1 Mux).
All trademarks are the property of their respective owners.
PCI Express compliance and interoperability testing is offered by the PCI Special Interest Group (PCI-SIG). The Compliance Workshop Program offers standardized device electrical and system testing for PCI Express systems, peripherals, and components. The program provides component and system manufacturers the opportunity to test new Intellectual Property (IP) for electrical performance and compatibility with other PCI Express products. Texas Instruments uses the PCI-SIG workshops to perform standardized PCIe tests which ultimately lead to inclusion on the PCI-SIG Integrators List. Products referenced on the Integrators List meet PCIe requirements and will provide a robust solution. The PCI-SIG compliance program is made up of several mandatory test procedures as well as an interoperability program.
The goal of this application note is to review the process and provide an understanding of the PCI-SIG Compliance Program, especially in the way that compliance testing relates to linear redrivers.