SNOA952 May 2016 FDC2112 , FDC2112-Q1 , FDC2114 , FDC2114-Q1 , FDC2212 , FDC2212-Q1 , FDC2214 , FDC2214-Q1
System ground configurations are differentiated by their use of either earth ground or local ground. For example, if the sensor PCB is connected to a battery and has no other connections to the external world, the observed performance is different than that of a system referenced to earth ground when parasitic capacitances are introduced. The location and size of the ground reference also makes a difference.