SNOAAA5 April   2024 DRV8220 , FDC1004-Q1 , LDC3114-Q1 , TMAG5131-Q1 , TMAG5173-Q1 , TMAG6180-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Automotive Door Handle Architectures
  6. 3Functional Demo Design
  7. 4Detailed Design Flow for Door Handle Functions
    1. 4.1 Door Open or Closed Detection With Magnetic Sensing
      1. 4.1.1 Demo Implementation of Open Close Detection Using TMAG5131-Q1
    2. 4.2 Deployable Door Handle Position Detection With Magnetic Sensing
      1. 4.2.1 Demo Implementation of Deployable Door Handle Position Sensing Using TMAG6180-Q1
    3. 4.3 Hand Proximity Detection With Capacitive Sensing
      1. 4.3.1 Overview of Capacitive Sensing Applications
      2. 4.3.2 Examples of Soft-Touch Detection Based on Capacitive Sensing in a Door Handle Demo
        1. 4.3.2.1 Touch Button
        2. 4.3.2.2 Door Handle
    4. 4.4 Push Button With Inductive Sensing
      1. 4.4.1 Inductive Push Buttons
      2. 4.4.2 Inductive Push Button Sensitivity
      3. 4.4.3 Target Material
      4. 4.4.4 Target Distance and Sensor Size
      5. 4.4.5 Design Example
  8. 5Summary
  9. 6References

Touch Button

Consider the touch button located to the (outside) right of the pull handle (to the left on the inside). The 1.4cm x 2.1cm rectangular sensor is positioned on the inside surface of the 5mm-thick polycarbonate plastic. If we assume this condition can be approximated by an idealized parallel-plate capacitor, we can expect the capacitance to be about C ≈ εoεrA/d = 8.85∙10-12∙5∙(0.014)∙(0.021)/0.005 = 2.17pF when a finger is pressing against the outer surface. This assumes the area of the finger pressing the outer surface is at least as large as the sensor on the inside surface of the polycarbonate.

We also might approximate the absence of any finger on the touch button as a parallel-plate capacitor with a separation distance much larger than the sensor dimensions. Following this assumption, suppose the distance d is 30mm. This can result in a capacitance of C ≈ εoεrA/d = 8.85∙10-12∙5∙(0.014)∙(0.021)/0.030 = 0.43pF.

How do these two approximate calculations compare to the demo? The plot in Figure 4-19 shows a plot of the demo's FDC1004 output versus time samples with a finger placed over the touch button between the 400th and 500th sample. Before the finger is applied, the FDC1004 reports the sensor capacitance is about 0.5pF to 0.6pF, which somewhat in agrees with our rough calculations. After the finger is placed over the button, the reported capacitance settles out to 2pF to 2.1pF, which is close to values from our approximate calculations above.

GUID-A35741A4-9CE4-4A0A-B9AA-33717F21317B-low.jpg Figure 4-19 Demo Touch Button: FDC1004 Reported Capacitance Before and After Finger is Applied