SNVA994A February 2022 – March 2023 LM5157 , LM5157-Q1 , LM51571-Q1 , LM5158 , LM5158-Q1 , LM51581 , LM51581-Q1
According to the theory of the peak current mode control, the slope of the compensation ramp must be greater than half of the sensed inductor current falling slope to prevent subharmonic oscillation at high duty cycle. Therefore, the following inequality in Equation 9 should be satisfied.
where
Typically 82% of the sensed inductor current falling slope is an optimal value of the slope compensation, which reflects to a margin of 1.6. If the inequality is failed, the inductance value of LM must be increased so that the falling slope can be smaller. If the LM inductance value is changed the peak current must be re-calculated and the device selection must be re-examined. In this example, the inequality is verified in Equation 10, Equation 11, and Equation 12.