SNVAA43 March 2023 LM5157 , LM5157-Q1 , LM51571-Q1 , LM5158 , LM5158-Q1 , LM51581 , LM51581-Q1
The MOSFET switch (SW) on the primary side must have a drain-source voltage rating greater than the maximum input voltage plus the output voltage. The drain-source voltage is calculated as follows:
A 30% margin must be added to the previous value.
The current through the MOSFET is calculated as follows:
For the power dissipation the RMS current is needed:
In this case, a MOSFET is chosen that is rated for 80 V, 10 A.