SNVAA88 December 2023 LM51581-Q1 , TPS1H000-Q1 , TPS92642-Q1
Figure 4-8 shows the voltage waveform of the LED driver output in yellow and the corresponding voltage on the coaxial cable in green. The figure shows that the LEDs are pulsed correctly and the voltage waveform on the coaxial cable is as expected. The figure shows the waveforms for a LED current of 2.5 A , a pulse width of 4 ms and a high-side switch current limit of 250 mA.