SPRUJ07 august 2023 TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
This migration guide describes the hardware and software differences to consider when moving between F2837x/F2807x and F28P65x C2000™ MCUs. This document shows the block diagram between the two MCUs as a visual representation on what blocks are similar or different. It also highlights the features that are unique between the two devices for all available packages in device comparison table. To facilitate application and hardware migration between F2837x and F28P65x devices, the PCB hardware section provides guidance on how to proceed with the common 176-pin package. A supplemental topic was included with recommendations for designing a 100-pin hardware that works for both F2837x and F28P65x 100-pin devices for early development of F28P65x application using F2837x 100-pin device. The digital general-purpose input/output (GPIO) and analog multiplex comparison tables show pin functionality between the two MCUs. F2807x is a single CPU, 120MHz variant of F2837x with only the 176-pin and 100-pin packages availble. The device comparison table only compares the superset F2837x device that has the complete set of peripherals and pins. Consult the F2807x datasheet for the more information on the available peripherals and pins if this will be used in migration. This serves as a reference for hardware design and signal routing when considering a move between the two devices. Lastly, the F28P65x software support is only in EABI format. The EABI migration is discussed in Section 5.