SPRUJD0 July   2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1

 

  1.   1
  2. 1Abstract
  3.   Trademarks
  4. 2Contributions to Power
  5. 3How to Use the Tool
    1. 3.1 Use Case
  6. 4Results Sheet
    1. 4.1 Some Specific Pre-loaded Use Case Results
      1. 4.1.1 ARM Only
      2. 4.1.2 Superset
      3. 4.1.3 3MegaPixel Front Camera
  7. 5Revision History

Contributions to Power

The SoC power is typically considered to have two different components – dynamic power and leakage.(2)

  • The dynamic power is computed based upon two numbers for the IP – max power and idle power (both scaled to the voltage). The dynamic power is computed as the weighted average of the max and idle power: Pdyn=Pmax×Utilization+Pidle×(1-Utilization)
    • For background: Dynamic power is typically computed as fCV². Consider a clock signal on a pcb that is driven from a CMOS output to a CMOS input. Dynamic power is computed based upon the (a) frequency of the signal – f; (b) the capacitance of the input load and the pcb trace capacitance – C; and (c) the voltage swing of the signal – V.
    • Within the tool, the user can select the frequency for some IP as well as the IP’s utilization. The frequency and utilization are obviously linked; as the frequency decreases, the utilization will need to increase to maintain the same activity. Therefore, a function that requires 40% loading on an IP will have nearly the same power if the frequency is cut in half and the utilization doubles to 80%.
  • The leakage power is computed based upon voltage, junction temperature, and manufacturing process variation. While the process and voltage have strong effects on the leakage power, the leakage power increases exponentially with Tj.
    • For background, a CMOS transistor is considered to have two states: (a) ON in which the channel between source and drain is conducting; and (b) OFF in which the channel is non-conductive between the source and the drain. Leakage power arises because the OFF state can allow a trickle of current to cross the channel.

There is a third component of the SoC power – that is, analog or bias currents. These currents are not considered in this tool because in almost all cases the power contributed from these sources is negligible to the overall power.