SPRZ544B March   2023  – December 2024 AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1

 

  1.   1
  2. 1Usage Notes and Advisories Matrices
    1. 1.1 Devices Supported
  3. 2Silicon Usage Notes and Advisories
    1. 2.1 Silicon Usage Notes
      1.      i2351
      2.      i2372
      3.      i2424
    2. 2.2 Silicon Advisories
      1.      i2049
      2.      i2062
      3.      i2097
      4.      i2134
      5.      i2189
      6.      i2196
      7.      i2199
      8.      i2208
      9.      i2249
      10.      i2278
      11.      i2279
      12.      i2310
      13.      i2311
      14.      i2312
      15.      i2366
      16.      i2371
      17.      i2120
      18.      i2137
      19.      i2190
      20.      i2253
      21.      i2373
      22.      i2383
      23.      i2401
      24.      i2407
      25.      i2409
      26.      i2410
      27.      i2376
      28.      i2399
      29.      i2413
      30.      i2414
      31.      i2419
      32.      i2420
      33.      i2421
      34.      i2422
      35.      i2423
      36.      i2431
      37.      i2435
  4.   Trademarks
  5.   Revision History

Usage Notes and Advisories Matrices

Usage Notes Matrix lists all usage notes and the applicable silicon revision(s). Advisories Matrix lists all advisories, modules affected, and the applicable silicon revision(s).

Table 1-1 Usage Notes Matrix
MODULE DESCRIPTION SILICON REVISIONS AFFECTED
AM62Ax 1.0
Boot i2372 — ROM doesn't support select multi-plane addressing schemes in Serial NAND boot YES
OSPI i2351 — OSPI: Controller does not support Continuous Read mode with NAND Flash YES
PLL i2424 — PLL: PLL Programming Sequence May Introduce PLL Instability YES
Table 1-2 Advisories Matrix
MODULE DESCRIPTION SILICON REVISIONS AFFECTED
AM62Ax 1.0
BCDMA i2431 — BCDMA: RX Channel can lockup in certain scenarios YES
Boot i2366 — Boot: ROM does not comprehend specific JEDEC SFDP features for 8D-8D-8D operation YES
Boot i2371 — Boot: ROM code may hang in UART boot mode during data transfer YES
Boot i2410 — Boot: ROM may fail to boot due to i2409 YES
Boot i2413 — Boot: HS-FS ROM boots corrupted ROM boot image YES
Boot i2414 — Boot: Ethernet PHY Scan and Bring-Up Flow doesn't work with PHYs that don't support Auto Negotiation YES
Boot i2419 — Boot: When disabling deskew calibration, ROM does not check if deskew calibration was enabled YES
Boot i2420 — Boot: XSPI Boot time is not consistent in SFDP mode YES
Boot i2421 — Boot: fatTiny GPT handling causes data abort YES
Boot i2422 — Boot: ROM timeout for MMCSD filesystem boot too long YES
Boot i2423 — Boot: HS-FS ROM applies debug access restrictions to all address space covered by the efuse controller firewall YES
Boot i2435 — Boot: ROM timeout for eMMC boot too long YES
c71x i2199 — C71x: SE returning incorrect data when non-aligned transposed stream crosses AM1 circular buffer boundary YES
C7x i2120 — C71x: SE returning incorrect data when non-aligned transposed stream crosses AM1 circular buffer boundary YES
C7x i2376 — C7x: SE/SA/HWAOPEN receives corrupted template following two back to back VPUT/MVC instructions YES
C7x i2399 — C7x: CPU NLC Module Not Clearing State on Interrupt YES
CSI_RX i2190 — CSI_RX_IF may enter unknown state following an incomplete frame YES
CPSW i2208 — CPSW: ALE IET Express Packet Drops YES
CPSW i2401 — CPSW: Host Timestamps Cause CPSW Port to Lock up YES
DSS i2097 — DSS: Disabling a layer connected to Overlay may result in synclost during the next frame YES
ECC_AGGR i2049 — ECC_AGGR: Potential IP Clockstop/Reset Sequence Hang due to Pending ECC Aggregator Interrupts YES
Interrupt Aggregator i2196 — IA: Potential deadlock scenarios in IA YES
MCAN i2278 — MCAN: Message Transmit order not guaranteed from dedicated Tx Buffers configured with same Message ID YES
MCAN i2279 — MCAN: Specification Update for dedicated Tx Buffers and Tx Queues configured with same Message ID YES
MMCHS i2312 — MMCHS HS200 and SDR104 Command Timeout Window Too Small YES
OSPI i2189 — OSPI: Controller PHY Tuning Algorithm YES
OSPI i2249 — OSPI: Failing OSPI DDR PHY Internal Pad Loopback and No Loopback timing modes YES
OSPI i2383 — OSPI: 2-byte address is not supported in PHY DDR mode YES
PRG i2253 — PRG: CTRL_MMR STAT registers are unreliable indicators of POK threshold failure YES
PSIL i2137 — PSIL: Clock stop operation can result in undefined behavior YES
RAT i2062 — RAT: Error Interrupt Triggered Even When Error Logging Disable Is Set YES
RESET i2407 — RESET: MCU_RESETSTATz unreliable when MCU_RESETz is asserted low YES
USART i2310 — USART: Erroneous triggering of timeout interrupt YES
USART i2311 — USART Spurious DMA Interrupts YES
USB i2134 — USB: 2.0 Compliance Receive Sensitivity Test Limitation YES
USB i2409 — USB: USB2 PHY locks up due to short suspend YES
VPU i2373 — VPU: VPU's interrupt is not routed to A53 YES