SWCU185G January 2018 – June 2024 CC1312PSIP , CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
While stop mode is not actually a transfer mode, stop is a valid value for the mode field of the control word. When the mode field has the stop value, the μDMA controller does not perform any transfers and disables the channel if enabled. The μDMA controller updates the control word to set the mode to stop at the end of a transfer. This mode can be useful in scatter-gather operations.