All trademarks are the property of their respective owners.
The TMP126EVM allows users to evaluate the performance of the TMP126 digital temperature sensor. The EVM comes in a USB stick form factor, with an onboard MSP430F5528 microcontroller that interfaces with both the host computer and the TMP126 device using an I2C interface. The module is designed with perforations between the sensor and host controller on the EVM board. The perforation allows the user flexibility in their evaluation:
Table 2-1 details the contents of the EVM kit. Contact the Texas Instruments Product Information Center nearest you if any components are missing. TI highly recommends that users check the TI website at http://www.ti.com to verify that they have the latest versions of the related software.
Item | Quantity |
---|---|
TMP126EVM | 1 |
Figure 3-1 shows an image of the TMP126EVM with some of the hardware features of the design labeled.