SNVAA17 April 2021 LM25180-Q1 , LM25183-Q1 , LM25184-Q1 , LM5180 , LM5180-Q1 , LM5181-Q1
All trademarks are the property of their respective owners.
The following test conditions apply to the results found in this document:
The LM5180 EVM was modified as shown in Figure 1-1 and in Table 1-1. First, the 10 μH EMI filer inductance was changed to 4.7 μH. The smaller inductor has a higher self resonant frequency (SRF) and, therefore, less parasitic capacitance. The parasitic capacitance of the inductor will by-pass the high frequency noise around the inductor, thus reducing the effectiveness of the EMI filter. A high SRF is desired for an EMI filter inductance in order to maintain the low-pass characteristic to the highest possible frequency. An additional filter capacitor, C3a, is added to bring the filter cut-off frequency back to near the value obtained with the 10 μH inductance.
In every fly-back transformer, switching noise on the primary side is couple to the secondary by the inter-winding capacitance. Unless a dedicated path is provided for this current, it will flow through any extraneous path to get back to the primary side. This common mode current will flow in an unnecessarily long path back to the primary side and show up as increased EMI. C1 is used to connect the primary and secondary grounds, providing a controlled path for this current while maintaining the D.C. isolation of the secondary output. Selecting, or designing, a transformer with low inter-winding capacitance will also help to reduce this noise contribution. The copper shield shown in Figure 1-2 is also helpful by capturing and shunting any capacitive noise current from the transformer windings back to the primary ground.
Finally, the snubber circuit capacitors, C8 and C10, were increased in value to help damp the ringing that occurs between the parasitic capacitance at the SW node and the transformer inductance. Ringing will also occur on the secondary side when the output diode turns off. This ringing will affect both conducted and radiate EMI, and should be damped as much as possible without affecting the operation of the regulator or unduly reducing the system efficiency.
The modified schematic shown in Figure 1-1, was used for all of the testing in this document. Modified components are shown in the red circles and in Table 1-1. The details of T1 and C3a are shown in Figure 1-2 and Figure 1-3. For more information, see the LM5180-Q1 Single-Output EVM User's Guide.
Reference | Modification |
---|---|
C3a | Added C3a; same value and location as C3; 0.1 μF |
L2 | Changed from 10 μH, Würth, 744042100 to 4.7 μH Würth, 744042004 |
C8, C10 | Changed value of both capacitors from 22 pF to 100 pF |
T1 | Wrap transformer with copper shielding tape. Shield grounded at one point on primary side. |
C1 | Install C1. 1000 pF, 2kV, 1206, X7R |