Chris Oberhauser66
In my previous post, I introduced the LDC calculator tool, which you can download here. It can calculate a number of useful parameters for an Inductive Sensing application.
LDC devices use inductors to sense the movement of conductive targets. At TI, we commonly use spiral traces routed on a printed circuit board (PCB) to form sensing inductors. WEBENCH® Coil Designer is a useful online tool that can help you design a sensor inductor and also generate a layout.
The racetrack inductor designer tool is another useful designer in the LDC tools spreadsheet. While the racetrack inductor designer only calculates sensor parameters and does not generate a layout, it is quick to use. Simply click Racetrack Inductor Designer on the Contents tab of the LDC calculator tool, or click the Racetrack_Inductor_Designer tab, as shown in Figure 1. You’ll wind up on the tab shown in Figure 2.
The LDC calculator tool is pretty accurate – typically a physical sensor will be within 10% of the calculations. For racetrack-shaped sensors, however, the accuracy may degrade when the ratio of the long side to the short side is greater than 4.
The first step in the process to design a sensor is to determine the PCB manufacturing limitations. Table 1 shows an example of limits from one PCB manufacturer.
Sensor Parameter | Value | Comments |
---|---|---|
PCB minimum trace width/space | 0.125 mm (5 mil) | Fabrication limitation |
Via minimum pad size | 0.6 mm (24 mil) | Fabrication limitation |
Via minimum hole size | 0.25 mm (10 mil) | Fabrication limitation |
Sensor minimum inner diameter | 0.825 mm (21 mil) | 0.6 mm + 2 × 0.125 mm One via pad + two trace spaces |
Stack-up thickness between layers | 0.80 mm (32 mil) | Desired PCB thickness |
Copper thickness | 0.5-1.0 oz-Cu |
You now need to know a few system limitations – what is the maximum possible size of the sensor, and how close the target can be to the sensor. I’ve summarized the values for an example system in Table 2.
Sensor Parameter | Value | Comments |
---|---|---|
Maximum sensor diameter | 9mm (315mil) | Mechanical constraint |
Target closest distance | 1.8mm | Based on system mechanicals |
For this example, I will use the LDC1612 and comply with the limitations from Table 1 and Table 2. Figure 3 shows the calculating region of the racetrack coil designer. I placed a number to the left of each parameter so you can follow me as I walk through each setting below.
Next, follow these steps to calculate a basic sensor design:
After entering your numbers, you may need to adjust the number of turns or the sensor capacitance. After trying several settings, I wound up with the values shown in Table 3. I chose 130 pF for the sensor capacitor so that I could safely use a 10% tolerance part.
Sensor Parameter | Value |
---|---|
Sensor capacitance | 130 pF |
Layers | 2 |
Turns | 14 |
Outer diameter | 9.0 mm |
Ratio of long edge to short edge | 1 |
Spacing between traces | 5 mil |
Width of trace | 5 mil |
PCB thickness | 32 mil |
Copper thickness | 1.0 oz-Cu |
Because the sensor’s electrical parameters change when the target is close, you need to verify that the sensor is still within the valid operating range of the LDC when this occurs. With the closest target distance of 1.8 mm, my sensor has the electrical specifications shown in Table 4, which are within the LDC1614’s operating region.
Sensor Inductance from Target Interaction | L' | 2.380µH |
Sensor Frequency with Target Interaction | fRES' | 9.049MHz |
Rp with Target Interaction | RP' | 4.90kΩ |
Q Factor with Target | Q' | 36.3 |
The LDC tool spreadsheet has a lot more uses. In my next post, I’ll review the LDC0851 calculator tab.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated