8 Revision History
Changes from Revision B (August 2022) to Revision C (July 2024)
- Added descriptions of items found in DLPC900REF-SW
Go
- Updated GUI software image to latest version.Go
- Added DLP200 Fault and
DMD Communication Error to the list of
status items.Go
- Added DMD Faults status section to System Settings.Go
- Updated Source Settings Tab and Display Settings Tab
images.Go
- Added note that names in Figure 4-11 and Figure 4-12 do not appear in the GUI.Go
- Updated Pattern Settings Panel image and added LED Controls invert
function description.Go
- Added Peripheral Panel to accommodate new Debug
section.Go
- Added Peripherals Tab
Go
- Added Debug Tab sectionGo
- Added information about the amount of patterns the DLPC900 can
holdGo
- Added section on reprogramming controller to support a different
DMDGo
- Added section on how to program an EDIDGo
- Changed the pinout table in DLPC900 UART Headers
sectionGo
- Added new section for pin J30Go
- Updated the mating part numbers in External Parallel Video
Connector sectionGo
Changes from Revision A (April 2022) to Revision B (July
2022)
- Changed all instances of legacy terminology to Primary and
Secondary throughout this document.Go
- Added note: heartbeat is present even if no DMD is
present.Go
- Changed J12 HOLDBoot jumper description to "BOOTHold"
jumper.Go
- Added Controller Board and DMD Board Assembly
instructions.Go
- Updated to Secondary terminology
for Secondary Present and Ready Status
item.Go
- Added a note East/West flip is permanently on for dual controller
designs.Go
- Updated to Primary-Secondary terminology in Deleting Images
Go
- Updated to Primary-Secondary terminology in Section 4.9.1.2
Go
Changes from Revision * (December 2020) to Revision A (April 2022)
- Changed GUI version to 5.0 and
added firmware 6.0Go
- Changed Image files default location and added selection
clarificationGo
- Changed the DLPC900REF-SW linksGo
- Added Standby wait period and commands accepted
information.Go
- Added note that the user must make sure the correct firmware is
programmed for the DMD EVM attached.Go
- Changed System Memory Test
to Internal Memory Test
Passed.Go
- Added note requiring an Update LUT command to resume operation after
stopping DMD Idle Mode.Go
- Added a note explaining IDX errors.Go
- Added steps 1 and 2 to clarify this exampleGo
- Clarified step 1 and added step 2 in Section 4.9.1
Go
- Updated step 1 and added step 2 in Deleting Images
Go
- Added step 11 and clarified phrasing and the directory of step 3 in
Section 4.9.1.2
Go
- Updated steps 1 and 2 in Section 4.9.1.3
Go