SBAA347 June 2022 AMC1300 , AMC1300B-Q1 , AMC1301 , AMC1301-Q1 , AMC1400 , AMC3301 , AMC3301-Q1 , TLV6002 , TLV9002
The following AC sweep shows the AC transfer characteristics of the single-ended output. Using the previously-calculated cutoff frequency illustrated in the last equation, shows that the simulation closely matches the simulation. Since the AMC3301 has a gain of 8.2 V/V and a gain of 0.778 V/V is applied with the differential to single-ended conversion, the gain of 16.11 dB shown in the following image is expected.