SBAA415 April 2020 PCM6240-Q1 , PCM6260-Q1 , PCM6340-Q1 , PCM6360-Q1
When multiple PCM6xx0 EVMs are connected to a single I2C bus, each EVM must have a unique I2C address. The I2C address is set by pullups and pulldowns on the Control and GPIO Selection at the underside of the board, as shown in Figure 20. Placement of the resistors in this section, as shown in Table 1, controls the I2C address of each PCM6xx0 device.
ADD1 | ADD0 | I2C SLAVE ADDRESS (BINARY) | ||
---|---|---|---|---|
1 | 0 | 1 | 0 | |
Not Installed | Installed | Not Installed | Installed | 1001 000 |
Not Installed | Installed | Installed | Not Installed | 1001 001 |
Installed | Not Installed | Not Installed | Installed | 1001 010 |
Installed | Not Installed | Installed | Not Installed | 1001 011 |