SBAA532A February 2022 – March 2024 ADS1119 , ADS1120 , ADS1120-Q1 , ADS112C04 , ADS112U04 , ADS1130 , ADS1131 , ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B , ADS1158 , ADS1219 , ADS1220 , ADS122C04 , ADS122U04 , ADS1230 , ADS1231 , ADS1232 , ADS1234 , ADS1235 , ADS1235-Q1 , ADS124S06 , ADS124S08 , ADS1250 , ADS1251 , ADS1252 , ADS1253 , ADS1254 , ADS1255 , ADS1256 , ADS1257 , ADS1258 , ADS1258-EP , ADS1259 , ADS1259-Q1 , ADS125H01 , ADS125H02 , ADS1260 , ADS1260-Q1 , ADS1261 , ADS1261-Q1 , ADS1262 , ADS1263 , ADS127L01 , ADS130E08 , ADS131A02 , ADS131A04 , ADS131E04 , ADS131E06 , ADS131E08 , ADS131E08S , ADS131M02 , ADS131M03 , ADS131M04 , ADS131M06 , ADS131M08
Bridges can also be constructed with more than one active element. Figure 2-5 shows a sensor with two active elements placed in different branches and on opposite sides of the bridge. This is known as a half bridge.
Equation 7 calculates VOUT for the bridge with two active elements in opposite branches shown in Figure 2-5:
Similar to the bridge with one active element, Equation 7 shows that VOUT is proportional to VEXCITATION and ΔR when ΔR is small. Moreover, the VOUT equation for both bridge types has a ΔR term in the denominator, resulting in the same non-linearity seen in Figure 2-3.
However, the important difference between a single-active-element bridge and a bridge with two active elements is the sensitivity. In the latter case, VOUT is two times larger for a given VEXCITATION. This larger output signal doubles the dynamic range compared to the single-active-element bridge, resulting in a better ADC measurement.