SBAA532A February   2022  – March 2024 ADS1119 , ADS1120 , ADS1120-Q1 , ADS112C04 , ADS112U04 , ADS1130 , ADS1131 , ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B , ADS1158 , ADS1219 , ADS1220 , ADS122C04 , ADS122U04 , ADS1230 , ADS1231 , ADS1232 , ADS1234 , ADS1235 , ADS1235-Q1 , ADS124S06 , ADS124S08 , ADS1250 , ADS1251 , ADS1252 , ADS1253 , ADS1254 , ADS1255 , ADS1256 , ADS1257 , ADS1258 , ADS1258-EP , ADS1259 , ADS1259-Q1 , ADS125H01 , ADS125H02 , ADS1260 , ADS1260-Q1 , ADS1261 , ADS1261-Q1 , ADS1262 , ADS1263 , ADS127L01 , ADS130E08 , ADS131A02 , ADS131A04 , ADS131E04 , ADS131E06 , ADS131E08 , ADS131E08S , ADS131M02 , ADS131M03 , ADS131M04 , ADS131M06 , ADS131M08

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Bridge Overview
  5. 2Bridge Construction
    1. 2.1 Active Elements in Bridge Topologies
      1. 2.1.1 Bridge With One Active Element
        1. 2.1.1.1 Reducing Non-Linearity in a Bridge With One Active Element Using Current Excitation
      2. 2.1.2 Bridge With Two Active Elements in Opposite Branches
        1. 2.1.2.1 Eliminating Non-Linearity in a Bridge With Two Active Elements in Opposite Branches Using Current Excitation
      3. 2.1.3 Bridge With Two Active Elements in the Same Branch
      4. 2.1.4 Bridge With Four Active Elements
    2. 2.2 Strain Gauge and Bridge Construction
  6. 3Bridge Connections
    1. 3.1 Ratiometric Measurements
    2. 3.2 Four-Wire Bridge
    3. 3.3 Six-Wire Bridge
  7. 4Electrical Characteristics of Bridge Measurements
    1. 4.1 Bridge Sensitivity
    2. 4.2 Bridge Resistance
    3. 4.3 Output Common-Mode Voltage
    4. 4.4 Offset Voltage
    5. 4.5 Full-Scale Error
    6. 4.6 Non-Linearity Error and Hysteresis
    7. 4.7 Drift
    8. 4.8 Creep and Creep Recovery
  8. 5Signal Chain Design Considerations
    1. 5.1 Amplification
      1. 5.1.1 Instrumentation Amplifier
        1. 5.1.1.1 INA Architecture and Operation
        2. 5.1.1.2 INA Error Sources
      2. 5.1.2 Integrated PGA
        1. 5.1.2.1 Integrated PGA Architecture and Operation
        2. 5.1.2.2 Benefits of Using an Integrated PGA
    2. 5.2 Noise
      1. 5.2.1 Noise in an ADC Data Sheet
      2. 5.2.2 Calculating NFC for a Bridge Measurement System
    3. 5.3 Channel Scan Time and Signal Bandwidth
      1. 5.3.1 Noise Performance
      2. 5.3.2 ADC Conversion Latency
      3. 5.3.3 Digital Filter Frequency Response
    4. 5.4 AC Excitation
    5. 5.5 Calibration
      1. 5.5.1 Offset Calibration
      2. 5.5.2 Gain Calibration
      3. 5.5.3 Calibration Example
  9. 6Bridge Measurement Circuits
    1. 6.1 Four-Wire Resistive Bridge Measurement with a Ratiometric Reference and a Unipolar, Low-Voltage (≤5 V) Excitation Source
      1. 6.1.1 Schematic
      2. 6.1.2 Pros and Cons
      3. 6.1.3 Parameters and Variables
      4. 6.1.4 Design Notes
      5. 6.1.5 Measurement Conversion
      6. 6.1.6 Generic Register Settings
    2. 6.2 Six-Wire Resistive Bridge Measurement With a Ratiometric Reference and a Unipolar, Low-Voltage (≤ 5 V) Excitation Source
      1. 6.2.1 Schematic
      2. 6.2.2 Pros and Cons
      3. 6.2.3 Parameters and Variables
      4. 6.2.4 Design Notes
      5. 6.2.5 Measurement Conversion
      6. 6.2.6 Generic Register Settings
    3. 6.3 Four-Wire Resistive Bridge Measurement With a Pseudo-Ratiometric Reference and a Unipolar, High-Voltage (> 5 V) Excitation Source
      1. 6.3.1 Schematic
      2. 6.3.2 Pros and Cons
      3. 6.3.3 Parameters and Variables
      4. 6.3.4 Design Notes
      5. 6.3.5 Measurement Conversion
      6. 6.3.6 Generic Register Settings
    4. 6.4 Four-Wire Resistive Bridge Measurement with a Pseudo-Ratiometric Reference and Asymmetric, High-Voltage (> 5 V) Excitation Source
      1. 6.4.1 Schematic
      2. 6.4.2 Pros and Cons
      3. 6.4.3 Parameters and Variables
      4. 6.4.4 Design Notes
      5. 6.4.5 Measurement Conversion
      6. 6.4.6 Generic Register Settings
    5. 6.5 Four-Wire Resistive Bridge Measurement With a Ratiometric Reference and Current Excitation
      1. 6.5.1 Schematic
      2. 6.5.2 Pros and Cons
      3. 6.5.3 Parameters and Variables
      4. 6.5.4 Design Notes
      5. 6.5.5 Measurement Conversion
      6. 6.5.6 Generic Register Settings
    6. 6.6 Measuring Multiple Four-Wire Resistive Bridges in Series with a Pseudo-Ratiometric Reference and a Unipolar, Low-Voltage (≤5V) Excitation Source
      1. 6.6.1 Schematic
      2. 6.6.2 Pros and Cons
      3. 6.6.3 Parameters and Variables
      4. 6.6.4 Design Notes
      5. 6.6.5 Measurement Conversion
      6. 6.6.6 Generic Register Settings
    7. 6.7 Measuring Multiple Four-Wire Resistive Bridges in Parallel Using a Single-Channel ADC With a Ratiometric Reference and a Unipolar, Low-Voltage (≤ 5 V) Excitation Source
      1. 6.7.1 Schematic
      2. 6.7.2 Pros and Cons
      3. 6.7.3 Parameters and Variables
      4. 6.7.4 Design Notes
      5. 6.7.5 Measurement Conversion
      6. 6.7.6 Generic Register Settings
    8. 6.8 Measuring Multiple Four-Wire Resistive Bridges in Parallel Using a Multichannel ADC With a Ratiometric Reference and a Unipolar, Low-Voltage (≤ 5 V) Excitation Source
      1. 6.8.1 Schematic
      2. 6.8.2 Pros and Cons
      3. 6.8.3 Parameters and Variables
      4. 6.8.4 Design Notes
      5. 6.8.5 Measurement Conversion
      6. 6.8.6 Generic Register Settings
  10. 7Summary
  11. 8Revision History

Bridge Overview

A Wheatstone bridge is a circuit used to measure a change in resistance among a set of resistive elements. The circuit has two parallel resistive branches that act as voltage dividers for the excitation voltage, VEXCITATION. The output of each resistor divider is nominally at VEXCITATION divided by two. With no applied load, the change in the resistance of the elements, ΔR, is equal to zero. Assuming an ideal system where the nominal resistance of each element is R, each voltage divider is at the same potential and the differential bridge output voltage, VOUT, is zero. When a load is applied, one or more of the elements changes resistance such that ΔR ≠ 0 Ω. This causes a change in VOUT that can be calculated very precisely by making a differential measurement across the bridge. Figure 1-1 shows the basic configuration of a simple bridge circuit using resistive elements.

GUID-20211110-SS0I-HCWL-6TLD-MW1P9DDRKW1K-low.svg Figure 1-1 Basic Configuration of a Simple Bridge Circuit

The basic bridge circuit is constructed using resistive elements with a single variable element in the bridge. This element is a resistive transducer that translates some physical parameter into a change in resistance. If this change in resistance is proportional to a change in the physical parameter, measuring ΔR yields an accurate representation of the physical property being sensed. While this document focuses on bridges using resistive elements, it is possible to construct a bridge using inductive or capacitive elements as well.

Bridge operation can be better understood by analyzing each side of the bridge in more detail. For example, the right side of the bridge in Figure 1-1 looks like the voltage divider circuit shown in Figure 1-2:

GUID-20211110-SS0I-ZVTJ-MGG6-GT9ZKC4NKXCP-low.svg Figure 1-2 A Resistive Element Measured as a Voltage Divider

Equation 1 calculates VOUT with respect to ground for the system in Figure 1-2:

Equation 1. V O U T =   V E X C I T A T I O N R + R R + R + R = V E X C I T A T I O N R + R 2 R + R

Assuming VEXCITATION = 6 V, R = 3000 Ω, and ΔR = 3 Ω, Equation 1 can be used to calculate that VOUT = 3.0015 V. Then, the voltage across R is calculated to be VR = VEXCITATION - VOUT = 2.9985 V. This yields a voltage across ΔR of VΔR = VOUT - VR = 0.003 V. While Equation 1 works in theory to calculate VOUT, VR, and VΔR, a real system must measure VOUT and VR to be able to derive VΔR. This can introduce additional challenges due to the limitations of standard measurement equipment.

For example, a simple 4-digit multimeter used to measure VOUT and VR could produce rounding errors that affect the calculation of VΔR: if the multimeter rounds VOUT = 3.0015 V up to 3.002 V and VR = 2.9985 V down to 2.998 V, then VΔR = 0.004 V; or, if VOUT is rounded down to 3.001 V and VR is rounded up to 2.999 V, then VΔR = 0.002 V. Both of these cases yield a measurement error of 1 mV relative to a 3-mV signal, or ±33% error. Ultimately, the 4-digit multimeter does not have enough resolution to consistently determine the precise value of ΔR by measuring across either resistive element in the divider.

For better results, the single-ended measurement shown in Figure 1-2 is changed to a differential measurement by placing the resistive transducer in a bridge configuration. In Figure 1-3, the bridge uses a second resistive path in parallel with the transducer path. With no applied load, ΔR = 0 Ω and VOUT = 0 V.

GUID-20211110-SS0I-TZJ5-ZJH4-M5CFN5TQDXZB-low.svg Figure 1-3 A Simple Bridge Using a Differential Measurement Across Two Resistive Paths

Equation 2 calculates the differential output voltage for the system shown in Figure 1-3 assuming R1 = R2 = R3 = R and R4 = R + ΔR.

Equation 2. V O U T =   V E X C I T A T I O N R + R 2 R + R - R 2 × R =   V E X C I T A T I O N R 2 × 2 R + R  

Using the same values from the single-ended example where VEXCITATION = 6 V, R = 3000 Ω, and ΔR = 3Ω, VOUT is now calculated to be 1.49925 mV. Importantly, the same 4-digit multimeter can measure VOUT much more precisely and on a millivolt scale as either 1.499 mV (rounded down) or 1.500 mV (rounded up). Measuring VOUT differentially in a bridge configuration yields a measurement error of <1 μV relative to a 1.5-mV signal, or 0.067%. This result occurs because a bridge configuration enables direct measurement of ΔR instead of a comparative measurement between ΔR and R. A direct measurement also enables VOUT to be amplified to get a larger input signal to the ADC. This amplification enables higher-resolution measurements of smaller values of ΔR.

One challenge with a single active resistive element bridge is that it has an inherent non-linearity in the measurement. Different bridge constructions have different non-linearities, and some topologies eliminate this inherent non-linearity. This is discussed in more detail in the next section.