SBAA532A February 2022 – March 2024 ADS1119 , ADS1120 , ADS1120-Q1 , ADS112C04 , ADS112U04 , ADS1130 , ADS1131 , ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B , ADS1158 , ADS1219 , ADS1220 , ADS122C04 , ADS122U04 , ADS1230 , ADS1231 , ADS1232 , ADS1234 , ADS1235 , ADS1235-Q1 , ADS124S06 , ADS124S08 , ADS1250 , ADS1251 , ADS1252 , ADS1253 , ADS1254 , ADS1255 , ADS1256 , ADS1257 , ADS1258 , ADS1258-EP , ADS1259 , ADS1259-Q1 , ADS125H01 , ADS125H02 , ADS1260 , ADS1260-Q1 , ADS1261 , ADS1261-Q1 , ADS1262 , ADS1263 , ADS127L01 , ADS130E08 , ADS131A02 , ADS131A04 , ADS131E04 , ADS131E06 , ADS131E08 , ADS131E08S , ADS131M02 , ADS131M03 , ADS131M04 , ADS131M06 , ADS131M08
Digital filters also have a specific frequency response that can affect how the signal is converted by the ADC. This response depends on the frequency of the input signal because the digital filter is collecting modulator outputs over a period of time. Figure 5-6 shows the frequency response of the different sinc filters in the ADS1235 at ODR = 50 SPS.
While not shown in Figure 5-6, the bandwidth of the ADS1235 sinc filters is significantly lower than the ODR. For example, the sinc1 cutoff frequency is only 22.1 Hz at ODR = 50 SPS. Therefore, bridge measurement systems that need to sample signals with higher frequency components require a higher ODR or a wider bandwidth digital filter. Refer to the Digital Filter Types in Delta-Sigma ADCs application note for more detailed information on this topic.
Another consideration of the digital filter frequency response is the rejection of specific frequencies. Figure 5-7 shows the frequency response for the ADS1235 FIR filter at ODR = 20 SPS, while Figure 5-8 zooms in on the response at 50 and 60 Hz.
As Figure 5-8 shows, this digital filter frequency response is designed to reject 50-Hz and 60-Hz frequencies. For example, the ADS1235 attenuates an input signal at 50 Hz or 60 Hz (with up to a ±2 Hz deviation) by 94 dB. This is particularly useful to reduce line-cycle noise in the system. Moreover, the ADC digital filter can help reject this noise whether it couples in from the system supply or comes from other line-induced EMI.