SBAA607A December 2023 – January 2024 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P4 , AM263P4-Q1 , AMC1303M2520 , AMC1305L25 , AMC1306M25 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
Figure 3-1 shows the first compensation method, where an additional phase locked clock signal with a software configurable phase delay is used. For this compensation method the phase-shifted clock signal CLKOUT_delay is used as the clock input to SD0_CLK of the Sigma-Delta Filter Module (SDFM). For other types of Delta-Sigma Modulators and MCUs e.g. C2000 MCUs, the compensation method follows the same principle.
The implementation of a second phase-shifted clock signal offers the highest degree of freedom and user configurability. This means that various values for minimum hold time th(MIN) of various isolated modulators can be compensated by a simple change to the phase-shift value in software. The clock signals rising edge at the SD0_CLK input is phase-shifted such that the clocking signal complies with the data sampling point of the SDFM, as shown in Figure 3-2. The AM243x PRU_ICSSG PRU Timing Requirements in Sigma Delta Mode are 10 ns for minimum setup time tsu (SD_D-SD_CLK) (MIN) = 10 ns and 5 ns for minimum hold time th(SD_CLK-SD_D) (MIN) = 5 ns. This creates a need for compensation to maintain correct acquisition at the data input SDx_D with reference to the rising clock edge of the SDx_CLK signal as the AMC1306M25 minimum hold time th(MIN) is 3.5 ns, but 5 ns can be required. After this compensation method is applied, the 10-ns minimum setup and 5-ns hold timings for the Sigma Delta Mode of the AM243x PRU_ICSSG PRU timing requirements are met, see Figure 3-2.