SLAA828B March 2018 – August 2021 MSP430FR2000 , MSP430FR2032 , MSP430FR2033 , MSP430FR2100 , MSP430FR2110 , MSP430FR2111 , MSP430FR2310 , MSP430FR2311 , MSP430FR2422 , MSP430FR2433 , MSP430FR2512 , MSP430FR2522 , MSP430FR2532 , MSP430FR2533 , MSP430FR2632 , MSP430FR2633 , MSP430FR4131 , MSP430FR4132 , MSP430FR4133
MSP430 and LaunchPad are trademarks of Texas Instruments Incorporated.
All trademarks are the property of their respective owners.
The 10-bit ADC module of MSP430FR2xx and MSP430FR4xx products is shown in Figure 1-1. The ADC acquisition channel can directly sample the internal voltage reference (typically 1.5 V, see the data sheet for details), and the ADC reference voltage can be configured as the supply voltage. The ADC input channel detailed information can be found in the "ADC Channel Connections" table in the device data sheet. Configure the ADCINCHx bits in the ADCMCTL0 register as defined in the table to use a 1.5-V reference as the input voltage. The reference voltage for the ADC is configured as 000b for the ADCSREFx bits.
Equation 1 shows how to calculate the 10-bit ADC conversion results.
where
Set Vin to the on-chip 1.5-V reference source, set VR+ to VCC, and set VR- to VSS. Equation 2 shows the formula to calculate the supply voltage.
Compared with the traditional solutions, on-chip ADC detection solution has the following advantages:
This document lists the main factors that affect power consumption with the on-chip ADC sample solution in MSP430FR4xx/FR2xx devices with 10-bit ADC. The power consumption results are given with different configurations. This example uses the 1.5-V internal reference voltage. Because the ADC trigger signal does not stop or start the 1.5-V internal reference voltage automatically, software can enable the 1.5-V REF and wait approximately 30 µs before triggering the ADC in the RTC interrupt. Software can also stop the reference in the ADC conversion ready interrupt. The following test is based on this approach. Developers can optionally keep the internal reference enabled all the time at the expense of higher power consumption.
Some MSP430FR4xx and MSP430FR2xx devices have a 12-bit ADC with an internal reference voltage that can be turned on and off automatically during an ADC conversion. Besides this exception, the implementation of battery voltage measurement with these devices is similar to the devices with 10-bit ADC; however, implementation details are outside the scope of this document.
Two main MSP430 system clock sources are available: the internal 32-kHz low-frequency REFOCLK and the external crystal XT1CLK. Table 2-1 compares the power consumption of the system clocks DCOCLK and ACLK using these clock sources. Using the external XT1CLK as the system clock source results in outstanding power consumption.
Clock Source (1) | REFOCLK | XT1CLK |
---|---|---|
Sampling frequency (Hz) | 1 | 1 |
Power consumption (µA) | 19 | 1.2 |