SLAA870 February 2019 AFE7422 , AFE7444
First, program TXNCO0 to 100 MHz through the Advanced tab in the AFE74xx GUI. See Section 4.1.1.3 for programming instructions.
Next, program TXNCO1 to 10 MHz by using a configuration file to update the TXNCO1 registers. The configuration file containing the necessary register writes to program TXNCO1 to 10 MHz is found in Section 7.
Before issuing the command to switch from TXNCO0 to TXNCO1 as the active NCO, make sure that the trigger setting on the oscilloscope is set to trigger on the negative edge of the SDEN signal. Then, load the configuration file containing the SPI writes required to switch from TXNCO0 to TXNCO1. The register writes used to select the active TX NCO are located in Section 7. The oscilloscope triggers after the SPI command is sent, capturing the transition from TXNCO0 to TXNCO1.