SLAAEA3A March 2023 – September 2023 MSPM0C1106 , MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507 , MSPM0L1105 , MSPM0L1106 , MSPM0L1303 , MSPM0L1304 , MSPM0L1305 , MSPM0L1306 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346
Today, cordless power tools (such as drills, saws, and impact wrenches) and cordless garden tools (such as leaf blowers, string trimmers, and lawn mowers) are smaller, lighter, more efficient, and more powerful due to advancements in battery technology and motor control techniques. All of these cordless tools require a microcontroller (MCU) to control direct current through a motor, and depending on the application, the MCU can also control different operating modes and integrated LEDs. TI’s MSPM0 MCUs can meet these requirements with their high-performance features, broad portfolio, and diverse package sizes.
Cordless tool-related applications need to control a brushed-DC (BDC) or brushless-DC (BLDC) motor to apply dynamic torque at a constant speed (such as drills and saws), or a constant torque at a dynamic speed (such as blowers). In many designs, the user can adjust the speed of the motor while applying torque to the motor to perform an action, like cutting or drilling wood with a bit, blade, chain, or wheel. For these designs, the main components include:
An application can use TI devices for most of these components that use TI devices for the driver and power stage across a wide range of 3-phase BLDC motor voltages and powers.
Motor | MCU | Motor Voltage | Predriver | Power Stage, Inverter | Hall Sensor Feedback |
---|---|---|---|---|---|
Brushed-DC | MSPM0Lxx Arm Cortex M0+ 32 MHz MCUs or MSPM0Gxx Arm Cortex M0+ 80 MHz MCUs | 5.5 V to 60 V | H-bridge Gate Driver (DRV870x series) | MOSFET (CSD series) | Hall Sensor (DRV5xxx series) |
5 V to115 V | H-bridge Gate Driver (DRV877x series) | ||||
Brushless-DC | 3 V to 40 V | 3-phase BLDC Motor Driver (DRV831x series) | |||
4.5 V to 60 V | BLDC Gate Driver (DRV832x series) | MOSFET (CSD series) | |||
8 V to 100 V | BLDC Gate Driver (DRV835x series) | ||||
5 V to 100 V | BLDC Gate Driver (DRV8300x series) |
Texas Instruments' scalable MSPM0 MCU portfolio features an Arm® 32-bit Cortex-M0+ core with a maximum CPU speed of 32-MHz or 80-MHz, depending on the device. The pin-to-pin compatible portfolio covers 4 KB to 512 KB of flash memory with scalable analog integration and motor control modules. With extensive digital, analog, and interface integration, MSPM0 can provide a high-performance and robust option for motor control designs.
For basic BDC systems
Most entry-level power tools such as drills, drivers, jigsaws, circular saws, shop vacuums, and even some garden tools like the propulsion system in some electric mowers require a relatively inexpensive low-speed BDC motor.
In this type of system, the MCU performs a simple motor control algorithm to control the motor speed and direction while handling any motor faults. Typically, the MCU also acts as the main processor in the system to control other components such as LEDs or to communicate with other devices such as the battery management system (BMS) in the battery pack. Texas Instruments' 32-MHz MSPM0Lxx series is an option for these types of products.
Key feature requirements for MCUs in these applications:
Software functions performed on the MCU:
For sensored BLDC systems requiring high torque
Many high-performance power tools such as hammer drills and heavy-duty impact wrenches require a BLDC motor to achieve higher power, higher torque, longer lifetime and better efficiency compared to a BDC motor. Sensored BLDC motor applications are typically easier to implement because Hall-effect sensors, Hall elements, or rotary encoders detect the position of the motor regardless of the load conditions, which maintains reliable high-torque start-up and robust operation.
In this type of system, the MCU performs a motor control scheme by generating multiple configurable PWMs in the correct sequence based on feedback from the position sensors and measuring the motor current. Typically, the MCU also acts as the main MCU in the system to control other components such as LEDs or communicate with other devices such as the battery management system in the battery pack or onboard inertial measurement unit (IMU). With a maximum CPU speed of 80 MHz, advanced timers, integrated analog, enhanced communication interfaces, high-drive inputs and outputs (HDIOs), and CAN-FD interface, the MSPM0Gxx series meets these requirements and is a great choice for these types of products.
Key feature requirements for MCUs in these applications:
Software functions performed on the MCU:
For sensorless BLDC systems requiring high speed or small form factor
Outdoor products such as electric mowers, string trimmers, and leaf blowers and also power tools such as low-voltage electric screwdrivers require compact high-speed sensorless BLDC motors. Unlike sensored BLDC motors, these motors do not require position sensors, which saves board space and reduces packaging in designs that require a small form factor. However, sensorless BLDC motors are more challenging to implement than sensored BLDC motors because there are no position sensors to provide motor speed or position data during dynamic load conditions.
In this type of system, the MCU performs an advanced motor control scheme by generating multiple configurable PWMs in the correct sequence based on back electromotive force (BEMF) voltage feedback from the motor. BEMF can be measured using two comparators or calculated using a first-order differential equation (from sampled motor phase voltage and current) to detect when the motor changes states in a six-step commutation pattern. Additionally, a sensorless BLDC system requires a start-up method such as Initial Position Detection (IPD) to determine the position of the motor at rest, an open loop start-up method to not lose motor sync, and a robust hand off to closed-loop control once enough BEMF is detected. Since power tools can spin at high speeds, simultaneously sampling ADC phase voltages and currents at high speeds to minimize latency in the feedback loop is critical.
Furthermore, the MCU can control other components such as LEDs or communicate with other devices such as the battery management device in the battery pack, wireless radios, or other sensors. With a maximum CPU speed of 80-MHz, advanced timers, integrated analog peripherals, enhanced communication interfaces and high-drive inputs and outputs (HDIOs), the MSPM0Gxx series meets these requirements and is an option for these types of products.
Key feature requirements for MCU in these applications:
Software functions performed on the MCU:
Order a MSPM0 LaunchPad™ development kit today and a DRV83xxEVM today to start evaluating MSPM0 for a cordless power or garden tool design. Jump-start a design with MSPM0 code examples and interactive online trainings. The following links show resources that are also available:
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated