SLAAEF5 March 2024 MSPM0G1505 , MSPM0G1505 , MSPM0G1506 , MSPM0G1506 , MSPM0G1507 , MSPM0G1507 , MSPM0L1303 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1306-Q1
For the SM COM Tool, shown in Figure 3-1, it is used to control the source meter to run the battery testcase, and show the data measured by source meter. The record data is saved in excel with a name “time-SmData.xlsx”. If you want to recreate this part for software, you need to at least install NI_VISA. For hardware, you need to buy a USB to rs232 wire and a keithley 2602A source meter.
As the source meter is not a equipment purely made for BMS, pay attention that it has limitations on the BMS test. For example, it cannot support high current control with high voltage battery. It can trigger the AFE into protection mode with constant current control, because the battery voltage will change above the threshold set in the AFE.