SLAAEF5 March 2024 MSPM0G1505 , MSPM0G1505 , MSPM0G1506 , MSPM0G1506 , MSPM0G1507 , MSPM0G1507 , MSPM0L1303 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1306-Q1
The capacity learn part has three functions:
The key output parameters of the function are listed in Table 2-2.
Parameter | Comment |
---|---|
iGuageDominationFlg | When this flag is set, the u16MaxNomFullCap_mAh is generated and the SOC accuracy goes to an acceptable accuracy |
iq15CaliSoc_DEC | This parameter is used by Capacity learn part to record as the calibrated NomAbsSoc for further NomFullCap calculation, after ocvCaliFinishFlg is set. It is also used by Current gauge part to recalculate NomRemCap in the same cycle. |
u16CaliOcv_mV | Used to calibrate NomAbsSoc after ocvCaliFinishFlg is set. |
u16NomFullCap_mAh | This parameter is used by Capacity learn part to calculate SOH. It is also used by Current gauge part to calculate NomRemCap and discharge or charge cycles. |
u16MaxNomFullCap_mAh | This parameter is fixed once the first u16NomFullCap is get and used to calculate SOH. |
iq15SOH_DEC | Used to show the capacity decrease. |